Min_Current
Index.Sub | 2005.1H |
Data Type | Unsigned16 |
Access | Read/Write |
PDO Mappable | RX_PDO (1) |
Unit |
milliamperes (mA) |
Range |
0 to Max drive current |
Default Value | 0 |
Store Supported | Yes |
Description |
It sets the motor’s reduced current. The drive automatically reduces the current after a current reduction time at the end of the movement. This object is used for Open Loop. |
Notes |
|